|
If you have a heat pump that's over ten years old, now's the time to start thinking
about replacing it, not simply repairing it.
Why? Because today's generation of heat pumps are so efficient, they can often pay
for themselves through decreased utility bills.
According to the Trane Home Comfort Institute, heat pumps usually last from 12 to
15 years, depending on their use. Your present unit is beginning to show its age
when major components of the system such as the motor or compressor start making
unusual noises or when the service calls start mounting up. It's at this point that
you'll have to decide whether to repair the old system or replace it with a new
one.
In the short run, replacing a major component costs less than replacing the entire
system. In the long run, however, you may be missing an opportunity to greatly improve
the overall efficiency of your system and save significant amounts of money in operating
costs.
In recent years, heat pump manufacturers have made dramatic progress in increasing
the efficiency of their units. As a result, it may make more economic sense to invest
the money spent on repairs in a new, more efficient unit that will immediately lower
operating costs.
Eventually, the more efficient unit should pay for itself through decreased utility
bills. In the meantime, you'll gain the added benefits of greater reliability and
longer warranty protection.
When looking at a new system, remember that the efficiency of a heat pump is indicated
by two ratings, one for heating and one for cooling. The heating rating is called
the Heating Seasonal Performance Factor (HSPF), the cooling rating is called the
Seasonal Energy Efficiency Ratio (SEER). In both cases, the higher the number, the greater
the efficiency and the lower the operating costs.
In order to attain the rated efficiency of the new system, the Trane Home Comfort
Institute notes that it's important to replace both the outdoor unit (which includes
the compressor) and the indoor unit (which includes the blower and evaporator) at
the same time. Combining a new high efficiency outdoor unit with an old low efficiency
indoor unit will probably not result in optimum performance.
It's also important to select the correct size unit for your home. A competent heating
and cooling contractor, after a thorough inspection of your home, can determine
how much capacity is required to keep your home comfortable.
Following installation of the new system, many dealers offer service contracts that
call for periodic maintenance of equipment and, if needed, repairs. The cost of
such a contract is usually well worth the investment.
|