|
Today's generation of gas furnaces can boost indoor comfort levels at the same time
they cut heating bills.
Considering this combination of benefits, is it any wonder that so many homeowners
are replacing their old, inefficient units with these modern, high-tech models?
If you're thinking about replacing your old gas furnace, the Trane Home Comfort
Institute reminds you that selecting the right size furnace is important. A unit
that's too small will lack the ability to give you the comfort you want. A unit
that is too large will cost more to buy and operate.
The heating experts also remind you that the size of a gas furnace refers to its
heating capacity not its physical dimensions. The capacity of a heating system is
measured in BTUs (British thermal units) per hour.
The correct furnace size depends on the size of your home, its construction and
insulation, the way you use the house and the normal winter temperatures in your
area.
A qualified heating and cooling dealer can estimate the heat loss of your home by
measuring the amount of wall, roof and floor space exposed to the outside, and the
amount of insulation you have.
Using a mathematical formula that includes the desired indoor temperature and the
local outdoor temperature ranges, he can then recommend an appropriate size for
your new furnace.
In many cases, older homes have furnaces that are larger than necessary, and homeowners
are pleased to discover they can replace it with a smaller capacity unit.
This situation often exists because of the addition of significant amounts of insulation
or because of other energy conservation measures that have been taken to substantially
reduce the heat loss of the house.
The increased efficiency of today's gas furnace is another reason. For example,
a new, smaller furnace that's 90% efficient can produce as much heat as a larger
capacity furnace that's only 60% efficient.
The heating contractor can also tell you if any changes are needed in the venting
of the furnace. In most cases, the new furnace is placed in the same location as
the old and uses the same venting system. However, many of today's high-efficiency
gas furnaces can be vented out a side wall similar to a gas dryer.
If you're thinking about installing a new furnace, the Trane Home Comfort Institute
notes it's also a good time to think about adding accessories that can increase
comfort levels even more. These include an electronic air cleaner, a humidifier
and a programmable thermostat.
And, if you don't already have it, it's also a good time to think about adding central
air conditioning. Be sure to tell your heating contractor of your desire so that
he can match the needs of the cooling system with that of the gas furnace.
|