|
According to the Trane Home Comfort Institute, electronic air cleaners are usually
installed in the duct carrying air back to the furnace or air handler. A typical
disposable furnace filter captures only 10% to 15% of the contaminants, while electronic
air cleaners can remove many more of the undesirable airborne particles from the
air it filters.
Operation of the unit is fairly simple. First, air passes through a mesh-type filter
that catches large airborne particles. Smaller particles that get through the filter
pass through an ionizing section where they receive an electrical charge.
These charged particles then pass through plates that have an opposite charge that
attracts the particles like a magnet. The particles remain on the plates until the
air cleaner elements are washed. The result is a healthier, cleaner indoor environment.
|