|
An in-depth look at clean air |
|
There are a lot of things in the air that affect your family's health. Click to
choose from the clean air topics below and learn about each one. Then, see the many
ways that Trane can help with Trane Air™ - air that is filtered and cleaned, as
well as flawlessly heated, cooled and thoroughly conditioned. |
|
Pollen |
|
Pollen. It's inside. It's outside. You even carry it on your clothes. It can make
you miserable. Over 28 million Americans suffer from hay fever and allergies. And
in today's airtight homes pollen is even more difficult to remove. |
|
How can Trane help with pollen? |
|
Many people find some comfort by taking refuge in a well air-conditioned environment.
But now there's a revolutionary new way to filter up to 99.98% of the airborne particles,
including pollen and other allergens, and it's only available from Trane. It works
as an integral part of your home comfort system, and it's called Trane CleanEffects™. |
|
Smoke |
|
When that cigarette is put out, the smoke doesn't just go away. It lingers. Tobacco
smoke contains over 4,000 compounds that coat your home's interior with harmful
residue that can seriously aggravate allergies and conditions like asthma. |
|
How can Trane help with smoke? |
|
The best way to keep smoke out of your house is not to allow smoking inside. Ask
smokers to smoke outside. Another option to help remove smoke once it's in the house
is a whole-house air filtration system. The revolutionary new TRANE CleanEffects™
system works as part of your home's comfort system to remove up to 99.98% of the
particles, including some smoke, from your filtered air. |
|
Asthma |
|
If anyone in your family suffers from asthma, you know how important controlling
environmental conditions inside the home can be. From hot and cold to dusty or dry
air, the triggers are many, and options for improving your family's air can seem
hard to find. |
|
How can Trane help with asthma? |
|
The best treatment for asthma sufferers is the regular care of a doctor. Children
are especially sensitive to irritants, so make sure they're regularly screened.
Also, look into reducing exposure to particulates in the air that can aggravate
asthma symptoms. A TRANE CleanEffects™ whole-house air filtration system can make
the filtered air in your home up to 99.98% allergen-free. |
|
Pets |
|
Sure, you love them, but not the hair and dander they bring into your home. Even
the pets of the home's previous occupants can leave an uncomfortably sneezy, itchy
legacy. Regular grooming and washing can help, but once the particles are in the
air, they can cause an allergic reaction. |
|
How can Trane help with pets? |
|
Minimize your pet's access to couches and bedrooms. When looking for a pet, ask
a veterinarian about breeds that produce less allergy-causing dander. To decrease
the amount of symptom-causing particles in the air, consider a TRANE air cleaner
option that is many times more effective than the standard 1" filters common in
85% of homes. |
|
Dust |
|
It's everywhere . As long as people have lived indoors they've tried to remove it.
And no matter how clean your home, you always have it. In fact, the average home
generates 40 pounds of dust for every 1,500 square feet each year! |
|
How can Trane help with dust? |
|
You can remove as much dust from the air as possible before it settles. A whole-house
humidifier can help keep air from becoming too dry, which would allow dust to circulate
more easily. And the new TRANE CleanEffects™ is the industry's most effective whole-house
air filtration system, capable of removing up to 99.98% of the particles from the
filtered air. |
|
Home Furnishings |
|
Did you know your family's air is affected by carpeting? And couch? And bedding?
Not only are they great hiding places for dust, smoke, and allergens, they can also
release potentially harmful pollutants that come from the processes used to manufacture
them. |
|
How can Trane help regarding home furnishings? |
|
Research the materials used to manufacture your furnishings and see if there are
any warnings about possible harmful exposure. Clean upholstery along with bed linens
regularly. To help filter out any particles or pollutants, consider a TRANE air
cleaner option that is many times more effective that the standard 1" filters common
in 85% of homes. |
|
Humid Air |
|
It doesn't need to be hot for humid air to make your family uncomfortable. Air that
is too moist for too long can allow potentially harmful bacteria, mildew and other
organic irritants to grow. |
|
How can Trane help with humid air? |
|
A Trane two-stage air conditioner or heat pump with a variable-speed furnace or
air handler can drastically improve your control over humidity levels in your home.
These variable-speed systems run longer at a slower speed for better temperature
control, but also to properly condition and dehumidify the air. |
|
Dry Air |
|
Air that is too dry for too long can be as uncomfortable as humid air, only for
different reasons. Not only can it be hard on your family's skin, but dry air -
because it lacks heavy moisture droplets - allows dust and other particulate matter
to circulate more easily through your home. |
|
How can Trane help with dry air? |
|
For atmospheric conditions that lead to dry indoor air, a whole-house humidifier
can give you greater control over the moisture level in your home, greatly increasing
your comfort. Often, dry air is also caused by furnaces or air handlers that are
improperly sized to a home. Trane makes both in sizes that are designed to meet
the comfort demands of any home. |
|
Hot and Cold Spots |
|
The living room is freezing. The bedrooms are roasting. Uneven temperatures keep
the air in many homes from being as clean and comfortable as possible. Air that
is too hot tends to hold more moisture, while cold air holds less. This hot and
moist air provides an atmosphere that promotes the growth of organic irritants,
while the cooler, drier air allows them to circulate more easily. |
|
How can Trane help with hot and cold spots? |
|
The most important part of creating a consistent indoor comfort level is making
sure your heating and cooling system is the right size for your home. Your independent
Trane dealer can perform what's known as a load calculation, which determines the
proper size of each component of your home comfort system. |